Any differences between KE02Z-20M and KE02Z-40M except MAX CPU frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any differences between KE02Z-20M and KE02Z-40M except MAX CPU frequency

Jump to solution
2,073 Views
CashQQJ
Contributor I

I've got a FRDM-KE02Z board, but I can only find FRDM-KE02Z40M board in NXP website.

Also I can only find KE02Z64xxx4 (no KE02Z64xxx2) SDK support in MCUXpresso IDE 11.2.

So anyone could tell me the main differences between these two MCU except MAX CPU frequency?

CAN I use KE02Z64xxx4 SDK to programm KE02Z64xxx2?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
2,065 Views
mjbcswitzerland
Specialist V

Hi

Apart from respecting the maximum frequency the same code can be run on the FRDM-KE02Z and the FRDM-KE02Z40M.

Try also the open source uTasker project on Github for easy development, lots of features and simulation of the KE02 board/device: https://github.com/uTasker/uTasker-Kinetis
It has a setup specifically for the FRDM-KE02Z.

Pre-built binaries at
- https://www.utasker.com/kinetis/FRDM-KE02Z40M.html
- https://www.utasker.com/kinetis/FRDM-KE02Z.html

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training or product development requirements

 

View solution in original post

0 Kudos
Reply
2 Replies
2,051 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

Except for the CPU frequency, please refer to below differences.

 

danielchen_0-1601880813272.png

 

Regards

Daniel

 

0 Kudos
Reply
2,066 Views
mjbcswitzerland
Specialist V

Hi

Apart from respecting the maximum frequency the same code can be run on the FRDM-KE02Z and the FRDM-KE02Z40M.

Try also the open source uTasker project on Github for easy development, lots of features and simulation of the KE02 board/device: https://github.com/uTasker/uTasker-Kinetis
It has a setup specifically for the FRDM-KE02Z.

Pre-built binaries at
- https://www.utasker.com/kinetis/FRDM-KE02Z40M.html
- https://www.utasker.com/kinetis/FRDM-KE02Z.html

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training or product development requirements

 

0 Kudos
Reply