After Moving Vector Table Device Crashes on First IRQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

After Moving Vector Table Device Crashes on First IRQ

1,896 Views
pcpro178
Contributor III

I've updated my linker file, so that the IVT should be located at 0x2300.

MEMORY
{
m_flash_config (RX) : ORIGIN = 0x000022F0, LENGTH = 0x00000010
m_interrupts (RX) : ORIGIN = 0x00002300, LENGTH = 0x00000100
m_foo_data (RW) : ORIGIN = 0x00002400, LENGTH = 0x00000400
m_bar_data (RW) : ORIGIN = 0x00002800, LENGTH = 0x00000400
m_baz_data (RW) : ORIGIN = 0x00002C00, LENGTH = 0x00000400
m_qux_data (RW) : ORIGIN = 0x00003000, LENGTH = 0x00000400
m_text (RX) : ORIGIN = 0x00003400, LENGTH = 0x0003CC00
m_data (RW) : ORIGIN = 0x1FFFE000, LENGTH = 0x00008000
}

Upon launching the debugger I can see the IVT at 0x2300, as well as the implemented ISR vectors at their respective offsets, in the memory view.  My SCB->VTOR value is also set to the expected 0x2300.  The only other thing I see, which I can't explain, is that when I inspect __VECTOR_TABLE it's value is still 0x20006000.  I'm not sure if that's an issue or not.  I have only these four ISRs implemented:

  • ADC0_IRQn
  • PIT_IRQn
  • TPM2_IRQn
  • LPUART0_IRQn

Does anyone know what's wrong here?

Labels (1)
0 Kudos
Reply
2 Replies

1,725 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jim,

Can you tell me the tools and part number you are using?

I have checked the project which is created with KDS tools, this is the definition of __VECTOR_TABLE

If you locate the interrupt table in internal SRAM, in other words, "m_interrupts" is defined as SRAM address, of course, the __VECTOR_TABLE is also in SRAM, in other words, The __VECTOR_TABLE has the same value as "m_interrupts".

Hope it can help you

BR

XiangJun rong

/* Define output sections */
SECTIONS
{
  /* The startup code goes first into internal flash */
  .interrupts :
  {
    __VECTOR_TABLE = .;
    . = ALIGN(4);
    KEEP(*(.isr_vector))     /* Startup code */
    . = ALIGN(4);
  } > m_interrupts

0 Kudos
Reply

1,725 Views
pcpro178
Contributor III

Thanks for the quick reply.  I'm using the MKL17Z256VLH4 and Kinetis Design Studio v3.2.0.  I thought that my IVT was located in flash.  Does it need to be stored in RAM?  Perhaps that is the piece I am missing.  If so, how does the IVT normally get copied to RAM?

Oddly, in the map file, I can see that both m_interrupts and __VECTOR_TABLE are at address 0x2300.  When I look at address 0x2300 in the Memory window I can see my interrupt vectors.  However, vector 0 is address 0x20006000, which is the value of __VECTOR_TABLE when viewed in the Expressions window.  Interestingly, when the debugger initially launches SCB->VTOR is 0x2300, but when program execution stops due to the invalid ISV the value of SCB->VTOR is 0.

0 Kudos
Reply