Access ports wordwise

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Access ports wordwise

2,207件の閲覧回数
sionp
Contributor II

Hi,

         I would like to know whether we can write to multiple pins of a port in one instant by using some sort of write to port register where each bit of the register will be the port pin. After going through the documentation I was unable to find the same. For applications where the parallel buses can be used such as character LCD/ digital attenuators/potentiometers, it would be helpful.

ラベル(1)
3 返答(返信)

2,136件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Sion,

Yes, of course. Kinetis MCU's gpio is grouped into several port. There are up to 32 gpio in each port. There are also some 32 bit wide register to control these gpio. Write to there 32bit register can read/write pins simultaneously. Please see the GPIO chapter in reference manual.

Regards,

Jing

2,136件の閲覧回数
sionp
Contributor II

Hope GPIOx_PDOR registers are the one you are referring to. Since the API's were not using this register I was not able to find. Also the manual has got these registers hidden towards the end of the document in memory mapping section.

0 件の賞賛
返信

2,136件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is. And you can use GPIOx_PCOR and GPIOx_PSOR to make the work easier.

Regards,

Jing

0 件の賞賛
返信