AN4368 's several problems.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN4368 's several problems.

1,212 Views
ConstYu
NXP Employee
NXP Employee

I am now using AN4368, but found there are several problems like below.

1. it only support S19 with S3 formate(the default generated formate of CW), while the IAR generated S2 formate S19 file, so it need to make a transfer.

2. it can't support bin formate, it report unknown file.

0 Kudos
Reply
1 Reply

1,029 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Ningning,

Kinetis Bootloader can support bin format.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply