AN4368 's several problems.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN4368 's several problems.

1,213件の閲覧回数
ConstYu
NXP Employee
NXP Employee

I am now using AN4368, but found there are several problems like below.

1. it only support S19 with S3 formate(the default generated formate of CW), while the IAR generated S2 formate S19 file, so it need to make a transfer.

2. it can't support bin formate, it report unknown file.

0 件の賞賛
返信
1 返信

1,030件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Ningning,

Kinetis Bootloader can support bin format.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信