Hi, I am trying to get the an2295 bootloader up and working on a MK10DX128LH7. The idea is afterwards to modify it to work on CANbus, but first I am trying just to get it working on uart.
I am using the official zip file from the freescale site.
I am using CodeWarrior 10.6.
I have managed to compile the project, but when I start it (debug) I see it jumps to the Boot_ResetMCU function right after entering __main function.
I have read all forum post I could find on AN2295, but it does not seem to have helped me.
I am at my whits end with this project at the moment, so it would be great if somebody has some pointers (no pun intended *)
Thank you in advance, Lovro
解決済! 解決策の投稿を見る。
Hello Lovro Oreskovic:
Are you using the linker file that comes with the appnote software (AN2295_LinkerFile.lcf)?
If so, you may need to change the stack symbols at the end for this:
__BOOT_STACK_ADDRESS = . + 0x00001000;
__heap_addr = __BOOT_STACK_ADDRESS;
__heap_size = 0x00001000;
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi. do you solved the bootloader issue. i want to download the code through uart bootloader. could you kindly help to share it to me? thanks a lot.
I made a new workspace imported the project, and made the changes and it started working.
I am not really sure what was the difference, but it works now.
Thank you for the info, Lovro
Hi Lovro Oreskovic,
I'm a FAE from China. From above discussion, I see you have solved the bootloader issue. and I have a customer using MK10DX128VLL7 and asking for uart bootloader. so could you kindly help to share it to me? thanks a lot.
Hello Lovro Oreskovic:
Are you using the linker file that comes with the appnote software (AN2295_LinkerFile.lcf)?
If so, you may need to change the stack symbols at the end for this:
__BOOT_STACK_ADDRESS = . + 0x00001000;
__heap_addr = __BOOT_STACK_ADDRESS;
__heap_size = 0x00001000;
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Yes, I am using the linker file from the AN2295 project.
The address and size I had at first were 0x00008000, I tried a few different values, but i did not seem to help.
I am not really sure what the correct values should be.
Best regards,
Lovro