ADC Internal refernce voltage for K53n512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Internal refernce voltage for K53n512

721件の閲覧回数
kanimozhiraju
Contributor I

Hi, 

      I try to interface the temperature sensor with k53n512 and I need to know the reference voltage options to use for ADC.Please tell me that bandgap reference voltage can be used as ADC reference voltage.I tried with internal regulator voltage 1.75 and MCU AFE reference as 3V.But i need to to use 1.4 to 1.5V.Could anyone make a clarification for exact usage and various ways of reference voltage for Single ended ADC.I am using single ended ADC.Thanks in advance.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

537件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Per the data sheet, you may directly apply 1.4 to 1.5v on VREFH, please kindly refer to the following for details.

pastedImage_1.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

537件の閲覧回数
egoodii
Senior Contributor III

If you don't end up using the bandgap as a direct ADC reference, if you are willing to do two conversions you can use it as an indirect reference, as spelled out in AN3031 or my post:

On-chip temperature Calculations 

As noted in there, the bandgap stability is, however, 'not great', with an 80mV drift band (Vtdrift) across temp, which is > +/-3%.

0 件の賞賛
返信