I work with MKV58F24. When I send a buffer from PC - 128 bytes - I get only 9 on a micro controller side.
I tried a polling method
void UART_RecvPacket()
{
unsigned char chr;
/* If new data arrived. */
if ((kUART_RxDataRegFullFlag | kUART_RxOverrunFlag) & UART_GetStatusFlags(UART0))
{
chr = UART0->D;
rx_idx++;
printf("IDX = %d\n", (int)rx_idx);
}
}
As well as an interrupt method
void UART0_RX_TX_IRQHandler(void)
{
unsigned char chr;
/* If new data arrived. */
if ((kUART_RxDataRegFullFlag | kUART_RxOverrunFlag) & UART_GetStatusFlags(UART0))
{
chr = UART0->D;
rx_idx++;
printf("IDX = %d\n", (int)rx_idx);
}
}
The same result - only 9 bytes from 128 are received.
After receiving 9 bytes a status register does not indicates any problem
Set lower baud rate - 9600 (was 115200) - getting a bit more - 17 bytes.
What can be a problem?
OMG. I found the problem - for a debug purpose I used printf a lot in the code. It really slows down and stucks the program flow.
解決済! 解決策の投稿を見る。
Hi john71,
Looks like you've found the root cause.
Thanks for sharing.
Best Regards,
Robin
Hi john71,
Looks like you've found the root cause.
Thanks for sharing.
Best Regards,
Robin