2 ways traffic light with pedestrian crossing button traffic light

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2 ways traffic light with pedestrian crossing button traffic light

1,419件の閲覧回数
jordanliong95
Contributor I

Hi everyone sir,i'm needed help because don't know Using the FRDM-KL25Z board, with uVision 5 Keil compiler. 2 ways traffic light with pedestrian crossing button traffic light program. C programming

Thank you

leong

タグ(1)
0 件の賞賛
返信
1 返信

1,319件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi Leong,

 

There are some examples in the SDK, you can download it in this link: SDK Builder. Choose the FRDM-KL25Z board, select the IDE, in your case Keil MDK, and add all the middleware options so you can see all the examples.

 

pastedImage_2.png

 

For your specific application, there is an example you can check . See the gpio_led_output driver example, so you can see how to configurate a led. A button configuration for your application is also with the GPIO, but in this case it is an input (which in the led was an output).

 

You also can see the Reference Manual for more information of the peripherals configuration. The GPIO chapter is the 41, where you can see the Registers Configuration.

 

Best Regards,

Ricardo

0 件の賞賛
返信