kds update fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kds update fails

2,153件の閲覧回数
JimDon
Senior Contributor III

Fresh download 8/31:

Run "Check for Updates" select all:

 

An error occurred while collecting items to be installed

session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).

No repository found containing: osgi.bundle,ilg.gnuarmeclipse.core,2.9.3.201508190739

No repository found containing: osgi.bundle,ilg.gnuarmeclipse.debug.core,1.2.1.201508190739

No repository found containing: osgi.bundle,ilg.gnuarmeclipse.debug.gdbjtag.jlink,3.2.1.201508190739

No repository found containing: osgi.bundle,ilg.gnuarmeclipse.debug.gdbjtag.openocd,3.2.1.201508190739

No repository found containing: osgi.bundle,ilg.gnuarmeclipse.debug.gdbjtag.restart,1.3.1.201508190739

No repository found containing: osgi.bundle,ilg.gnuarmeclipse.packs.core,1.1.2.201508190739

No repository found containing: org.eclipse.update.feature,ilg.gnuarmeclipse.debug.gdbjtag.jlink,3.2.1.201508190739

No repository found containing: org.eclipse.update.feature,ilg.gnuarmeclipse.debug.gdbjtag.openocd,3.2.1.201508190739

No repository found containing: org.eclipse.update.feature,ilg.gnuarmeclipse.managedbuild.cross,1.14.1.201508190739

No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86_64,3.0.0

ラベル(1)
2 返答(返信)

1,634件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

This might be caused by the network issue. I have seen similar message on my machine too, and I tried several minutes again and it worked.

0 件の賞賛
返信

1,634件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jim,

as a heads up: there is a known issue (and workaround) if you try to update the GNU ARM Eclipse plugins, see Unable to Debug after KDS Update

As for your specific problem: can give a try de-selecting 'check all update sites' check box?

Workaround for “Installing Software has encountered a problem” in Eclipse | MCU on Eclipse

And again: for now I would not update the GNU ARM Eclipse plugins.

I hope this helps,

Erich