cannot install KDS if MCUXpresso is present

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cannot install KDS if MCUXpresso is present

ソリューションへジャンプ
954件の閲覧回数
gschelotto
Contributor V

Hi,

I've installed MCUXpresso IDE successfully on my Linux (debian) distribution but KDS installer failed at this point:

Screenshot from 2017-06-21 14-10-11.png

It seems that there's a problem with some PEmicro packages.

How can I address this issue? Should I remove the packages from MCUXpresso IDE and then reinstall KDS?

regards,

gaston

1 解決策
792件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Gaston,

If MCUXpresso was installed before KDS then use this command to install Kinetis Design Studio:

sudo dpkg -i --force-depends --force-overwrite kinetis-design-studio_3.2.0-1_amd64.deb

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
792件の閲覧回数
gschelotto
Contributor V

Erich, thanks for the hint but I cannot reproduce the suggested steps. In my case MCUXpresso was installed before KDS and KDS installer is delivered as .deb package instead the MCUXpresso .bin executable file.

Is there another workaround to fix it? (by tacking into account the installation order: 1st MCUXpresso, 2nd KDS IDE)

regards,

gaston

0 件の賞賛
返信
793件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Gaston,

If MCUXpresso was installed before KDS then use this command to install Kinetis Design Studio:

sudo dpkg -i --force-depends --force-overwrite kinetis-design-studio_3.2.0-1_amd64.deb

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信
792件の閲覧回数
gschelotto
Contributor V

It works! thank you Carlos and Erich for your help,

regards,

gaston

792件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Gaston,

the following thread should help you: https://community.nxp.com/thread/447699 

I hope this helps,

Erich

0 件の賞賛
返信