Using a FRDM-K66 and KDS. Was working OK but one time I plug it in and instead of a serial port, it appears as the mbed flash drive. How do I get it to go back to a serial port so I can use KDS again?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using a FRDM-K66 and KDS. Was working OK but one time I plug it in and instead of a serial port, it appears as the mbed flash drive. How do I get it to go back to a serial port so I can use KDS again?

492 Views
tedhale
Contributor I

Using a FRDM-K66 and KDS. Was working OK but one time I plug it in and instead of a serial port, it appears as the mbed flash drive. How do I get it to go back to a serial port so I can use KDS again?

0 Kudos
Reply
1 Reply

390 Views
mjbcswitzerland
Specialist V

Ted

Try OpenSDA Serial and Debug Adapter|NXP 

Regards

Mark


Which one did you have (DAP)? The ones they put on newer boards are quite a disaster in my experience - they get lost all the time and when they don't get lost they mostly don't work properly. Segger and P&E ones are fairly good if you can get them to load.
Professionals really needs a solution to connect to the SWD adapter to ensure no disturbance.
Strange that my really old boards (like KL02, KL05, KL25) just keep on working, even with Win 10....

0 Kudos
Reply