Using KDS3.2 for MKL27 custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using KDS3.2 for MKL27 custom board

3,112 Views
punitkumar
Contributor IV

Hi

I've developed custom board having KL27 MCU.

But can't find the option for this MCU while creating new project. Please tell me how to add support for KL27 on KDS3.2?

Labels (1)
0 Kudos
Reply
3 Replies

2,950 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Punit,

What about the part number of your chip? 

- If the below screenshot includes it , please install the KSDKv1.3, then you can choose it.

pastedImage_1.png

Please download the KSDKv1.3 at here :

Software Development Kit for Kinetis MCUs|NXP 

Please download the Kinetis SDK(REV 1.x) :

pastedImage_1.png

Then refer to "KDS_Users_Guide.pdf" ->4.2 Installing Kinetis SDK into KDS .

- if the screenshot haven't your chip , please tell me the part number .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,950 Views
punitkumar
Contributor IV

Thanks Alice

I've installed KSDK1.3 and already applied eclipse update, but still not showing KL27 MCU.

Untitled.png

0 Kudos
Reply

2,950 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Punit,

Please uninstall it , then install it again. Pay attention that , download and install the latest version .

For i have uninstall most of the update on my KDS, while it also can create project about KL27 , so

i think it is include when install KDSv3.2 .

BR

Alice

0 Kudos
Reply