TOWER-K64F120 +FREERTOS+SHELL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TOWER-K64F120 +FREERTOS+SHELL

2,456 Views
kooroshhajiani
Contributor III

Hello,

My target is TWR-K64F120 +TWR-SER2, using KDS and FREERTOS, I've created  a project which

is running OK and I can communicate over the serial link to a terminal using the DB9 connector on the SER2 board.

However I need to add SHELL  to this project. I noticed that there is a shell folder in the SDK that I'm using.

I'm not certain how to integrate the files in the shell folder into my project.

 

Is there a tutorial for this?

Please even if someone has done this for a bare metal (without any OS) your input is very valuable.

Any help is greatly appreciated.

 

 

 

Thanks,

Koorosh Hajiani   

Labels (1)
0 Kudos
Reply
4 Replies

2,137 Views
peterfurey
Contributor IV

Hi Koorosh,

I just asked a similar question and got an encouraging response. See my thread:

Can I easily extend FreeRTOS in the new Kinetis SDK v2.0?

Good luck!,

Peter

2,137 Views
kooroshhajiani
Contributor III

Hi Peter,

Finally got around doing it and it is working for me.

Many Thanks for your help.

Koorosh Hajiani

0 Kudos
Reply

2,137 Views
peterfurey
Contributor IV

That's good to hear. I'll give it a try next week.

0 Kudos
Reply

2,137 Views
kooroshhajiani
Contributor III

Hi Peter,

Thank you for your response, I will check it out and will let you know .

Thanks,

Koorosh Hajiani

0 Kudos
Reply