Processor Expert without Kinetis SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert without Kinetis SDK

1,947 Views
antonbizyaev
Contributor I

Hi! I can't create new project Processor Expert without Kinetis SDK... How I can this? Thx.

Labels (1)
0 Kudos
Reply
2 Replies

1,837 Views
BlackNight
NXP Employee
NXP Employee

Hi Anton,

for which device? That depends on the device you are using. Newer devices are supported by Processor Expert in combination with the SDK only.

Erich

0 Kudos
Reply

1,837 Views
antonbizyaev
Contributor I

Hi Erich,

I'am use FRDM KL03... I thing it is work with SDK only... Thx for answer! 

Anton

0 Kudos
Reply