Problem with KDS and Processor expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with KDS and Processor expert

1,789件の閲覧回数
michelmeunier
Contributor I

Hello,

I have an old project wich works fine for me (it uses FRDMKL25, the include MMA8451 and an external I2C component). I would like to start a similar new project, unfortunatly something is going wrong.

In my old project, they were only few components, but now with the new one after creating project, I have a lot of components. Some pictures to explain.

143850_143850.jpgP1.jpg

It's my old project with only the things I have added (MMA1,AS1,GI2C2...etc).

143851_143851.jpgP2.jpg

Just after creating the new project, I have strange components (osa1,clockman1,pin_mux..etc).

Also when I want to create an I2C connections, I can't select the pins:

143861_143861.jpgP3.jpg

My goal is to have a simple project as the old one!! I am not interested by pin_mux,intMan1 ...etc, it was working without that before.

Thanks for your help

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,631件の閲覧回数
michelmeunier
Contributor I

As usually Erich, you have the solution, thanks a lot.

Michel

0 件の賞賛
返信

1,631件の閲覧回数
BlackNight
NXP Employee
NXP Employee

This is because you are using the SDK.

Select 'none' during project creation:

none sdk.png

Erich

0 件の賞賛
返信