Problem with Code Area Highlighting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with Code Area Highlighting

1,359件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

 

Does anyone know why KDS shows areas code as being unused when they are controlled by pre-processor defines in the configuration properties -> C/C++ General -> Paths and Symbols -> Symbol tab ?

Areas of code controlled by defines in header files on the other hand are shown correctly.

 

See the following for the original problem report:

KDS Highlighting issues

 

Regards

 

Mark

 

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,248件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Mark,

I think it is that old (and annoying) Eclipse Indexer heuristics problem: see Fixing the Eclipse Index | MCU on Eclipse for the solution.

Erich

0 件の賞賛
返信