Problem while launching a debug for openSDA for KL25Z128VLK4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem while launching a debug for openSDA for KL25Z128VLK4

8,293 Views
bhupindersinghk
Contributor I

I am new to this board and KDS.

 

I was trying to execute a basic program to blink LED...

 

However while debugging the code through inbuilt openSDA a pop up windows shows as follows...

 

122061_122061.pngPicture1.png

 

I have also tried re-installing the P&E drivers.But nothing seems to work.

 

Also I am certainly sure that I am following the bootloader updating process properly.

 

I have also tried installing KDS in different system however same error occurs. Even i have tried on different kl25z128vlk4 board but nothing works.

 

Please suggest any possible solution for this problem as soon as possible.

Labels (1)
0 Kudos
Reply
14 Replies

7,830 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Which board do you use? FRDM-kl25? or your customer board ?

If the frdm-kl25, please drag the  file of "DEBUG-APP_Pemicro_v102.SDA" to the bootloader,

the plug in again the usb to  J7;

Then configure the debugger as this :

pastedImage_0.png

If still can not work , please take a screenshot about the process of your operate .

BR

Alice

0 Kudos
Reply

7,830 Views
bhupindersinghk
Contributor I

Thanks Alice_Yang for your reply. I am using FRDM-kl25z128vlk4.

My debugging window looks as below:

Picture1111.png

While debugging, KDS hangs at 61% as shown in following window:

Picture11.png

After this, P&E connection assistant window appears as shown below:

Picture1.png

Please suggest the possible solution for this.

0 Kudos
Reply

7,830 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Have you test   drag and past the attachment i have send you , then debug ?

0 Kudos
Reply

7,830 Views
bhupindersinghk
Contributor I

Yes, But no effect

1 more thing, I got a window after P&E connection assistant. It is as shown:

Capture.PNG

After i cancel the P&E connection assistant window, error in services launch sequence appears.

0 Kudos
Reply

7,830 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Please test it on other PC , check the problem is the PC or the board .

BR

Alice

0 Kudos
Reply

7,830 Views
bhupindersinghk
Contributor I

Hi Alice,

I have tried this on 2 PCs and even i have 2 boards. But I don't know why this problem occur.

Please help me out.

Regards,

Bhupinder singh Khural

0 Kudos
Reply

7,830 Views
bhupindersinghk
Contributor I

Hi Alice,

No.

The same result. It shows first error with pop up window of "P&E connecion assistant" (as shown in above reply). Then the other pop up window shows "Error in services launch sequence".

I don't know where the problem is. I have checked in other system as well as in another kl25z board but it is showing same error.

Please help me out.

Regards,

Bhupinder singh Khural

0 Kudos
Reply

7,830 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bhupinder,

It so strange ! From the debug configuration view , we can see the KDS has detect  the OpenSDA,

it should be connected well .At the Core option, does here have M0+? If have , please select M0+.

pastedImage_0.png

And what system do you used ?

If it still can not work , please take a picture for your board connection when debug .

BR

Alice

0 Kudos
Reply

7,830 Views
bhupindersinghk
Contributor I

Hello Alice,

There is no M0+ in core option.

I am using KDS 3.0.0 in windows 7 PC. And i have also tried on KDS 1.1.1 in another windows 7 system.

Here, below is the image for connection of frdm kl25z:

20160105_110450 (1).jpg

Regards,

Bhupinder singh khural

0 Kudos
Reply

7,830 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello

Please test my project on your side , use the KDS3.0 .

BR

Alice

0 Kudos
Reply

7,830 Views
bhupindersinghk
Contributor I

Hello,

I have tried your project on KDS 3.0 but it is not working.

Same things happened:

1. It showed P&E connection assistant window. (then i close this window and next thing happened)

2. Another window displayed that "Error in services launch sequence"

0 Kudos
Reply

7,830 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Oh, change one USB line .

0 Kudos
Reply

7,830 Views
bhupindersinghk
Contributor I

Hello,

By changing USB line do you mean to change the USB wire between board and system?

Regards,

Bhupinder singh khural

0 Kudos
Reply

7,830 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bhupinder,

"I have tried this on 2 PCs and even i have 2 boards" , what about the result ?

Does the other FRDM-KL25 board can work well ?

0 Kudos
Reply