Post-build commands

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Post-build commands

Jump to solution
3,047 Views
davidsherman
Senior Contributor I

I am trying to invoke objcopy directly, because I'm trying to generate two S-record files.  I have a specific section which will be located in an external EEPROM that needs to be stripped.  In the help file, it says multiple commands can be separated by semicolons. I can use either of these lines individually:

 

${cross_prefix}objcopy -O srec -j.nvdata --change-section-address .nvdata=0x0 program.elf program_eeprom.srec

${cross_prefix}objcopy -O srec -R.nvdata program.elf program_main.srec

 

Either of these alone will generate the correct S-record file.  However, if I try to put them both in the post-build command box with a semicolon separating them, nothing happens.

 

I could make a batch file that gets called and does these two operations, but I'd like to avoid having the path to the Gnu tools hard-coded in it.

Labels (1)
0 Kudos
Reply
1 Solution
3 Replies
2,796 Views
davidsherman
Senior Contributor I

Anyone?

0 Kudos
Reply
2,797 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
2,796 Views
davidsherman
Senior Contributor I

Thank you again, Erich!  I've bookmarked that site.  Looks like lots of good information there.

0 Kudos
Reply