MQX with PEG  tutorials

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX with PEG  tutorials

4,399 Views
danieljackmorle
Contributor III

Looking in to a project that requires graphics and I am trying to use with the K70 board or K60 board.

Which one will have the most tutorials or examples.

Labels (1)
0 Kudos
Reply
5 Replies

3,758 Views
DaveTonyCook
Contributor IV

Hi Zhang,

Your link https://community.freescale.com/docs/DOC-101586 provides no information

0 Kudos
Reply

3,758 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi dave,

this question was answered in 2014 and this article you mentioned is also old (written in 2014 too).  now it changes to version  5. I can't remember what exact it was two years ago.

If I am not wrong it should include a video at that time but now from my side the video can not be showed now.

as a suggestion you could leave your question to the article page, thus if  the author sees it he will know.

Jun

0 Kudos
Reply

3,758 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Daniel,

please refer thread as below:

https://community.freescale.com/docs/DOC-101586

==========================================

this answer is for you, if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

Zhang Jun

0 Kudos
Reply

3,758 Views
danieljackmorle
Contributor III

Do you have the files used in that demo on your web sight.

How do I get to the level in which I can do this using the kits.

Date: Fri, 10 Oct 2014 01:19:53 -0700

From: [email protected]

To: [email protected]

Subject: Re: - MQX with PEG tutorials

MQX with PEG tutorials

reply from ZhangJennie in Kinetis Design Studio - View the full discussion

Hello Daniel,

please refer thread as below:

https://community.freescale.com/docs/DOC-101586

==========================================

this answer is for you, if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

Zhang Jun

Did your question get answered?

If so, say thanks by clicking Correct Answer in the community thread!

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in Kinetis Design Studio by email or at Freescale Community

Following MQX with PEG tutorials in these streams:

Inbox

0 Kudos
Reply

3,758 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Daniel.

I suggest you check TWR-K70F120M + TWR-LCD-RGB  samples here:

PEG Software Product Line (GUI)|Freescale

PEG Medical Kiosk: Software offered 'As is', support provided on Freescale Communities only – Example PEG Application for the TWR-K70F120M + TWR-LCD-RGB.
Size (K): 2220 Format: exe Rev #: 1.0 Modified: 8/29/2012
FREESCALE
Download
Favorite
PEG MQX HVAC: Software offered 'As is', support provided on Freescale Communities only – Example PEG/MQX Application for the TWR-K70F120M + TWR-LCD-RGB.
Size (K): 2868 Format: exe Rev #: 1.0 Modified: 8/29/2012
FREESCALE
Download
Favorite
PEG MQX Web Security: Software offered 'As is', support provided on Freescale Communities only – Example PEG/MQX Application for the TWR-K70F120M + TWR-LCD-RGB.
Size (K): 2732 Format: exe Rev #: 1.0 Modified: 8/29/2012

Hope this helps!

==========================================

this answer is for you, if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

Zhang Jun

0 Kudos
Reply