LPCxpresso / KDS merging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCxpresso / KDS merging

2,102件の閲覧回数
piergiovannigor
Contributor II

Does someone made some other experiments in merging LPCxpresso and KDS ?

See my "crazy idea" May 27th 2015

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,711件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Giovanni,

Do you mean this: Merging NXP LPCXpresso IDE with Freescale Kinetis Design Studio, Processor Expert and Kinetis SDK | ...

?

So yes, I'm able to use LPCXpresso with Processor Expert and LPC and Kinetis boards, and I can use KDS with NXP ARM devices.

I mean they are both ARM, the toolchains are similar as well the IDE. The KDS one is mostly based on stock Eclipse and other open source components, so easier (in my view) to tweak for any custom devices or needs. The future will tell how the new NXP solution will look like, but as of today, you can merge them together yourself too.

Erich

0 件の賞賛
返信

1,711件の閲覧回数
piergiovannigor
Contributor II

Hi Erich,

    yes, I mean this.

The merged system works, but not all is ok, particularly for the selection of devices and drivers for debug probes

The actual situation is as our discussion in last May.

I think that since Freescale and NXP now are the same thing, may be that in the near future there will be an unified tool,

Giovanni

0 件の賞賛
返信