KSD IDE to Connect/Attach

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSD IDE to Connect/Attach

2,169 Views
Toe
Contributor IV

Can the KDS IDE connect or attach to a MCU already running an application?  CW10.x could, but I haven't found that option for the debug configuration in KDS.

Labels (1)
0 Kudos
Reply
3 Replies

1,902 Views
BlackNight
NXP Employee
NXP Employee

Unfortunately not with Segger yet, see

The J-Link hardware debugging Eclipse plug-in | GNU ARM Eclipse

Note: due to some implementation issues in the startup sequence of the J-Link GDB server, which ignores the -noreset option and always issues a target reset, the Connect to running target option, although fully implemented in the plug-in, is not yet functional; we are working close with the SEGGER specialists to fix it as soon as possible;

I need to see if there is another option. What connection type are you using? P&E? OpenOCD?

Erich

0 Kudos
Reply

1,902 Views
Toe
Contributor IV

I'm using a P&E Multilink Universal for most development right now.

0 Kudos
Reply

1,902 Views
BlackNight
NXP Employee
NXP Employee

I quickly checked with P&E and did some tests, and the P&E connection does a reset too (like Segger), so does not work as intended.

I have contacted P&E and they are looking into it.

Where it works with KDS is with OpenOCD connection: for this I have 'Connect to running target' enabled:

pastedImage_0.png

Plus 'Load Executable' disabled:

pastedImage_2.png

But this does not really help you if you have a custom board with P&E Multilink, unless you would use an OpenOCD FRDM board to your board.

Erich