KL16 mcu SPI read/write NandFlash failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL16 mcu SPI read/write NandFlash failure

1,140件の閲覧回数
junwang1
Contributor II

I use below code to read ID of external NandFlash . The code is generated under KDS's PE tool.Every operation returns a wrong result. 0xFF, 0xC8.   The right result should be 0xC8, 0xD4.  I test sck output wave, should output 32 clock  pulses, but really only output 16 clock pulses. 

....................................

txbuf[0] = 0x9F;

txbuf[1] = 0x00;

SM2_ReceiveBlock(SM2_DeviceData, recv_buf, 2);

SM2_SendBlock(SM2_DeviceData, txbuf, 2);

  while (!SM2_GetBlockReceivedStatus(SM2_DeviceData))

  {

  SM2_Main(SM2_DeviceData);

  }

.....................

ラベル(1)
0 件の賞賛
返信
1 返信

1,029件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

can you please upload your demo project for this issue?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信