KL02 doesn't work standalone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL02 doesn't work standalone

1,815 Views
bitki
Contributor I

Hello,

 

I use Kinetis Design  Studio V2.0.0.My cpu conf. like this:

 

18193_18193.pngpastedImage_0.png

 

I'm using FRDM KL25 dev board for USBDM debugger. When I load program with USBDM flash programmer, nothing happened but in debug mode its working. What is the wrong? Thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,665 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Gokhan,

1) The USBDM is open to everyone, so the USBDM from different company have a little  difference ,

it usually used to CW, you should be sure whether yours can used to KDS.


2) In the FRDM-kl25 board , you can directly flash through the openSDA , it only need link use USB. You can try .


Best Regards

Alice

0 Kudos
Reply

1,665 Views
bitki
Contributor I

Thanks Alice,

I'm not using FRDM-kl25 board to develope, only using to programming extenal device. My custom board has MKL02Z32VFK4.

0 Kudos
Reply