KDS2.0 Can't import previously Deleted Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS2.0 Can't import previously Deleted Project

1,044件の閲覧回数
frankbannon
Contributor II

I renamed a project (say Project 2) and KDS kept creating .elf under previous name.  So, I closed then deleted the project (not files just from KDS work space).

I tried to import Project2 thinking the KDS would create the .elf with Project2 name.  However,..... when I try and import the Project2 KDS "sees" it, but "select box" for Project2 is in the background, I can't select it to import.

 

Any thoughts?

 

Regards,

 

Frank

ラベル(1)
0 件の賞賛
返信
1 返信

964件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

User also needs to change the ‘Artifact Name’ option after rename the project in order to generate ELF with new name. To do it, please:

1) Click on ‘Project’ Menu-> Properties

2) Click on C/C++Build > Settings

3) Click on ‘Build Artifact’ tab

4) Change the name in ‘Artifact name’, please see the attached screenshot.


Artifact Name.png


Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信