KDS + pydev on Mac fails (but works in Windows)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS + pydev on Mac fails (but works in Windows)

1,053 Views
rajbatra
Contributor IV

KDS 3.0 Mac OS, I installed pydev just fine from http://pydev.org/updates (via Install software under help).

 

However, when searching or picking a python interpreter - I get:

 

java.io.IOException: Cannot run program "/usr/local/bin/python3": error=0, spawn failed

 

This error occurs even on base python that Apple distributes.

 

This works fine on Eclipse Luna and KDS 3.0 for Windows.

 

Any idea why it doesn't work for Mac?

Labels (1)
0 Kudos
Reply
2 Replies

891 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

officially,  the supporting working platform for is KDS3.0

Host operating systems:

  • Windows® 7/8 (32 and 64-bit)
  • Linux® 64-bit (Ubuntu 10.04 (deb), RedHat/Centos 7 (rpm))
  • Mac OS 10.10 ("Yosemite")

are you sure you are using Mac OS 10.10 ("Yosemite") but not other lower version?

 


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

891 Views
rajbatra
Contributor IV

Yes, 10.10.3 is what I have.

As a work around I'm just using Windows...

-Raj

0 Kudos
Reply