KDS + pydev on Mac fails (but works in Windows)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS + pydev on Mac fails (but works in Windows)

1,049件の閲覧回数
rajbatra
Contributor IV

KDS 3.0 Mac OS, I installed pydev just fine from http://pydev.org/updates (via Install software under help).

 

However, when searching or picking a python interpreter - I get:

 

java.io.IOException: Cannot run program "/usr/local/bin/python3": error=0, spawn failed

 

This error occurs even on base python that Apple distributes.

 

This works fine on Eclipse Luna and KDS 3.0 for Windows.

 

Any idea why it doesn't work for Mac?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

887件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

officially,  the supporting working platform for is KDS3.0

Host operating systems:

  • Windows® 7/8 (32 and 64-bit)
  • Linux® 64-bit (Ubuntu 10.04 (deb), RedHat/Centos 7 (rpm))
  • Mac OS 10.10 ("Yosemite")

are you sure you are using Mac OS 10.10 ("Yosemite") but not other lower version?

 


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

887件の閲覧回数
rajbatra
Contributor IV

Yes, 10.10.3 is what I have.

As a work around I'm just using Windows...

-Raj

0 件の賞賛
返信