KDS & MKV5x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS & MKV5x

1,530 Views
andreacanepa
Contributor IV

I have read that the microprocessor of the MKV5xx series is compatible with IDE KDS.

But when I try to create a new project with KDS using Processor Expert I'm not available in choosing the MKV5x processor: there are only MKV1x and MKV3x.

Why? Are there any upgrades to install? I use KDS V 3.2.0.

Tags (1)
0 Kudos
Reply
2 Replies

1,363 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Andrea,

The new Kinetis devices such as KV5 are supported by SDK2. processor expert no longer supports for them.

There is a similar discussion regarding to pe support for KV5. Hope this can help you

https://community.nxp.com/message/822231 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,363 Views
andreacanepa
Contributor IV

Jennie, thank you for the answer.

Andrea.

0 Kudos
Reply