KDS  - Keil MDK-ARM integration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS  - Keil MDK-ARM integration

2,244件の閲覧回数
stank
Contributor I

Hi,

 

The latest version 3.0.0 of KDS theoretically supports
project’s export to Keil MDK-ARM.

Even when choosing during the project creation - "Target
compiler as Keil ARM C/C++ Compiler", there is no any .uvprojx
file created, which could be then used for the μVision.

 

There is some explanation available how to
use Keil with Processor Expert:

http://mcuoneclipse.com/2014/11/09/using-keil-%CE%BCvision-5-with-processor-expert/

but I would like to use KDS instead.

 

Do you know any proper way how to link my KDS
project with Keil MDK-ARM?

 

Thanks,

Stan

ラベル(1)
0 件の賞賛
返信
1 返信

1,754件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Stanislaw,

I think that the following post created by our colleague Erich Styger might be helpful for you, it explains how to use KDS with Keil IDE:

Tutorial: Using Kinetis Design Studio V3.0.0 with IAR and Keil IDE’s | MCU on Eclipse

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信