KDS Debugger Settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS Debugger Settings

1,138 Views
rabbitz
Contributor I

I am Code Warrior user, just satrt KDS shortly.

 

My target board is SWD debugging interface,  "MultiLink Universal RevC" is the debugger.

When I start debugging, it downloading firmware to the target, it comes  error message "Program file does not exist", but the .elf is existing,

 

Is there any tutoring document for KDS debugging settings?

 

Regards

Sam

Labels (1)
0 Kudos
Reply
1 Reply

1,050 Views
DavidS
NXP Employee
NXP Employee

Hi Sam,

What target board?

I have seen where the Debug Configuration for the PEMicro debugger firmware defaults to USB Multilink and you need to change it to OpenSDA.

Once in awhile I have also not had the ELF file pointed to in the C/C++ Application: enter in the Main tab window.  Usually Search Project... will find it.  If not then Browse... to it will work.

Regards,

David

0 Kudos
Reply