I'm using KDS 3.2.0 with a PEmicro multilink and a MK22FN512 MCU.
How do I set up the debugger to use the backdoor access key to unsecure the device without a mass erase? Is there a command I can pass in or a setting i'm missing in KDS?
Thanks,
已解决! 转到解答。
Hello Matt,
The P&E multilink doesn't support backdoor key function to unsecure.
About the detail answer , you can also check this thread :
And About the use the kientis unsecrity with backdoor , i recommend you refer to this doc :
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4507.pdf?fsrch=1&sr=2&pageNum=1
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Matt,
Does this can help you ?
Using a backdoor key to unlock security for Kinetis family MCU
Hope it helps
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Alice,
No, I can use the backdoor, I just wanted a way for PEMicro debugger to be able to use the backdoor key to unsecure the device without a mass erase. I do not see anything about the backdoor key in the KDS debugger settings. I know USBDM has an option to use the backdoor key in their standalone programmer.
Hello Matt,
The P&E multilink doesn't support backdoor key function to unsecure.
About the detail answer , you can also check this thread :
And About the use the kientis unsecrity with backdoor , i recommend you refer to this doc :
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4507.pdf?fsrch=1&sr=2&pageNum=1
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------