KDS 3.2.0 How to increase HEAP size without Processor Expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS 3.2.0 How to increase HEAP size without Processor Expert

2,064件の閲覧回数
isaotakashima
Contributor IV

I'm making the new project using Kinetis SDK 2.0 by KDS 3.2.0 for the TWR-K65F180M.

I cannot make the new Processor Expert project by KDS 3.2.0, then I made the Kinetis SDK 2.x project.

I can increase HEAP size by edit MK65FN2M0xxx18_flash.ld as below.

HEAP_SIZE  = DEFINED(__heap_size__)  ? __heap_size__  : 0x1000;    /* increase HEAP size from 0x0400; */

STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x0400;

 

Can I increase HEAP size by GUI?

 

Please advise as soon as possible.

 

Best regards,

Takashima

ラベル(1)
タグ(1)
1 返信

1,446件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Takashima,

No, there is no specific GUI. But you can specify the heap and stack size with the linker commands (or actually in the linker panel GUI), see

https://mcuoneclipse.com/2016/04/17/changing-heap-and-stack-size-for-nxp-kinetis-sdk-v2-0-gcc-projec...

I hope this helps,

Erich