K60F120M support in KDS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60F120M support in KDS?

1,367 Views
michael_wahler
Contributor III

Hi,

 

In the "New Kinetis Design Studio Project" wizard I only get to choose from two boards (FRDM-K64F and TWR-K64F120M). Is there support for the TWR-K60F120M board?

 

Michael

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,109 Views
BlackNight
NXP Employee
NXP Employee

Hi Michael,

Yes, use the MK60FN1M0xxx12 on the TWR-K60F120M:

pastedImage_0.png

The 'Boards' group lists for now only boards supported by the Kinetis SDK. The difference between the 'boards' list and the normal list is that with the boards you get the the pin muxing pre-configured for that particular board. But you can use any board with the Processor/devices listed.

Erich

0 Kudos
Reply