Hello All-
New to KDS and the Kinetis ecosystem but very experienced with Cortex controllers and Eclipse-based IDEs...
I've just installed KDS on both Windows 7 and Ubuntu 14.04, followed by the KSDK using the Eclipse "Install New Software..." mechanism on both OSs. In both cases, when creating a new KDS Project, the Kinetis SDK option remains grayed out.
I followed the instructions in the KDS release notes, including restarting Eclipse (and, just to be sure, both machines) - is there anything else that needs to be done?
Thanks,
Dave
解決済! 解決策の投稿を見る。
Hi,
the SDK supports only few processors. Which one did you try?
I expect you:
1) installed KDS
2) installed KSDK
3) installed the eclipse update from KSDK folder (KSDK_1.0.0\tools\eclipse_update\SDK_1.0.0-GA_Update_for_Eclipse.zip)
Hi,
the SDK supports only few processors. Which one did you try?
I expect you:
1) installed KDS
2) installed KSDK
3) installed the eclipse update from KSDK folder (KSDK_1.0.0\tools\eclipse_update\SDK_1.0.0-GA_Update_for_Eclipse.zip)
Hello Libor - Yes, I followed the steps you outlined. I was trying with the LK25Z64xxx4 processor, but I see now that only K2x, K6x and KV3x controllers are supported.
Thank you,
Dave