How do I integrate eGUI with KDS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I integrate eGUI with KDS?

1,246件の閲覧回数
DaveTonyCook
Contributor IV

Hi,

 

I've downloaded the following:

KDS v1.1.0

KSDK v1.0.0

eGUI

 

and I have the K70 TWR + LCD module etc.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

985件の閲覧回数
terry_lv
NXP Employee
NXP Employee

Hi,

     Currently, K70 is not supported in KSDK v1.0.0 (Now K64 and K22 are supported), which means a big effort if you want to use eGUI with KSDK.

     If just using eGUI in KDS, I think you can just create a eGUI project in KDS.

     KDS is also an IDE for development, not limited to KSDK development.

     Thanks~~

Best regards

Terry

0 件の賞賛
返信