How do I integrate eGUI with KDS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I integrate eGUI with KDS?

1,308 Views
DaveTonyCook
Contributor IV

Hi,

 

I've downloaded the following:

KDS v1.1.0

KSDK v1.0.0

eGUI

 

and I have the K70 TWR + LCD module etc.

 

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,047 Views
terry_lv
NXP Employee
NXP Employee

Hi,

     Currently, K70 is not supported in KSDK v1.0.0 (Now K64 and K22 are supported), which means a big effort if you want to use eGUI with KSDK.

     If just using eGUI in KDS, I think you can just create a eGUI project in KDS.

     KDS is also an IDE for development, not limited to KSDK development.

     Thanks~~

Best regards

Terry

0 Kudos
Reply