Hexiwear Docking Station

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hexiwear Docking Station

2,896 Views
majidrehman
Contributor I

Hi,

I am facing problem with Hexiwear Docking Station.

When I connect Docking Station with my PC, then always mass drive label shows "MAINTENANCE".

can anyone help me how to fix this problem.

 

 

Thanks,

Majid

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,559 Views
BlackNight
NXP Employee
NXP Employee

Hi Majid,

this means that you are in 'bootloader' mode (see https://mcuoneclipse.com/2016/07/12/hexiwear-teardown-of-the-hackable-do-anything-device/ ). This happens if you power on the docking station with the reset button pressed. Or for some reasons you have erased the DAPlink debug application?

- try the docking station without the Hexiwear

- make sure that the reset button(s) on the board are not pressed

- check the voltage level of the reset line, maybe you have a shortcut on your board

- Check the switches (see https://mcuoneclipse.files.wordpress.com/2016/07/cardboard.jpg )

In any case, you can use the onboard SWD cable to debug the Hexiwear.

I hope this helps,

Erich

0 Kudos
Reply

2,559 Views
majidrehman
Contributor I

actually when I connect docking station without Hexiwear then nothing happen meaning mass drive DAPLINK does not appears,

and when I connect Hexiwear with docking station and turn ON, then mass drive MAINTENANCE appears with following files,

DETAILS.txt and HELP_FAQ.htm

any suggestion ?

Thanks

Majid

0 Kudos
Reply