Hello, I cannot create a new project in kinetics design studio.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hello, I cannot create a new project in kinetics design studio.

2,364件の閲覧回数
rafaelzambrano
Contributor II

I am trying to create a Kinetics Design Studio project, by executing New>Project>KDS Project, then I followed the Project Wizard, when I clicked finish the files are not created.

 

The Project Explorer window is empty.

 

 

Also, Do the Design Studio tools support the TWR-K24F120M development board. When creating the new project the TWR-K24F120M is not in the list of boards. Is there a new release of the tools to include the TWR-K24F120M in the Kinetics Design Studio tools?

 

Thank you.

ラベル(1)
1 返信

2,222件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Rafael,

I tested creating a new project and TWR-K24F120M project, there is no problem, see attached two videos.

here is some points we need to pay attention:

1. make sure you have admin right of install and using KDS . it's necessary.

2. to avoid old file associations, remove .metadata folder under your workspace folder, then restart your project again. test same.

3. make sure you install the latest KDS version: KDS2.0

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KDS_IDE&nodeId=0152101E8C1EB4&fpsp=1&...

4. make sure you install all the available update:

install update.png

does this answer your question?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------