Floating Point on KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Floating Point on KDS

6,148件の閲覧回数
ciful
Contributor II

Good morning.

I'm using the sprintf function but it doesn't work with float and double type.

It works properly only with integer.

I found a lot of information on this problem, but referred to the codewarrior ide.

How it's possible to solve this in the kinetis dev system ?

 

Thanks.

Claudio

ラベル(1)
8 返答(返信)

4,622件の閲覧回数
syedidris
Contributor III

I did same as matherin,

but not getting float printing, I getting error like this,

plz anyone clarify this doubt.

Untitleddhgh.png

0 件の賞賛
返信

4,621件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Syed,

What processor are you using?  Looking at the errors it seems like KL03.

The above post were asking for printf/scanf with floating point support.  Is that what you want too?

If yes attached is an example project for the FRDM-KL03Z.

Note that KL03 on the Freedom board is limited to 32KByte flash and very limited to 2KByte of SRAM.

Because of that I had to increase the compiler optimization to get the linker to work.

Regards,

David

0 件の賞賛
返信

4,621件の閲覧回数
syedidris
Contributor III

David sir,

Thanks for your reply.

Actually I am a beginner, and yes you are right, I am using KL03 processor.

And I don't know about processor expert. I am trying to learn with demo codes provided with KDS3.0.0 IDE. when I am trying to print the float value like,

float a=2.4;

PRINTF("%f",a);

I am getting output as ' f ' only, so I searched on forum and enabled the option -u_printf_float with the following:

Properties -> C/C++ build -> Settings -> Cross ARM C Linker -> Miscellaneous -> Use float with nano printf

But, no change in the behavior of printf.

I will be thankful to you if you solve my problem

4,621件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Syed,

Please open your Properties of your project and add the following SCANF_FLOAT_ENABLE and PRINTF_FLOAT_ENABLE....recompile and run again.

ScreenHunter_216 Dec. 14 15.49.gif

Regards,

David

0 件の賞賛
返信

4,621件の閲覧回数
larrykoos
Contributor III

Claudio,

Did you ever get this to work? I cannot get the approach described in the Erich Styger article referenced above to work because his comments are referencing newlib-nano, not newlib. Any help would be appreciated.

Thanks,

Larry

0 件の賞賛
返信

4,621件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Semihosting (and printf()) depends on the library used.

Have a look at

Semihosting with GNU ARM Embedded (Launchpad) and Kinetis Design Studio | MCU on Eclipse

Do not forget to use the -specs=rdimon.specs linker option.

I hope this helps,

Erich

0 件の賞賛
返信

4,621件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Claudio,

Please take a look at the following post created by our colleague Erich Styger, it explains how to use printf() and scanf() with floating point:

printf() and scanf() with GNU ARM Libraries | MCU on Eclipse

Hope it helps.

Best regards!

Carlos

0 件の賞賛
返信

4,621件の閲覧回数
matherinewang
Contributor III

Hello,

I have add -u _printf_float to the linker options to enable float/double support to printf/sprintf(), but still can not work with float, any other configuarion needed?

pastedImage_0.png