FRDM K64F KDS PE SPI Clock Rate setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FRDM K64F KDS PE SPI Clock Rate setting

跳至解决方案
15,514 次查看
brianmohlman
Contributor III

Hello All,

 

I am starting a project using the FRDMK64F board. I have the core clocking set for the max of 120MHz and I have added the fsl_Dspi bean to the project and when I try to set the clock rate I get:

 

Description Resource Path Location Type

Timing setting failed in Clock configuration 2 - it is impossible to set the following items: selected value (Clock rate) K64Test  spiCom1/Clock rate Processor Expert Problem
(I have attached a screenshot)

I have tried setting is to several different clock rates (2MHz, 6MHz, 12MHz, 20MHz) with the same result. .Anyone point me to what I am doing wrong?

 

Best Regards,

 

Brian

标签 (1)
1 解答
14,053 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Brian,

Just like I said to Justin below , delete the unused clock configuration from  cpu component .

Hope this helps.

Regards,

Alice

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

23 回复数
1,621 次查看
brianmohlman
Contributor III

Alice,

Thanks for your help deleting all configurations except one fixed the issue.

Best Regards,

Brian

0 项奖励
回复
1,621 次查看
brianmohlman
Contributor III

*Justin not Jeff, my apologies Justin.....

0 项奖励
回复
1,621 次查看
justinc
Contributor II

All good :smileyhappy:

0 项奖励
回复