Error while Debugging the example code for FRDM-K82F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while Debugging the example code for FRDM-K82F

1,248 Views
mohammadgouse
Contributor I

I am testing the FRDM-K82F kit with sample codes, i am getting error while i am debugging it, screenshot of the output as follows

 

156228_156228.pngpastedImage_0.png

Need solution for this, I am using GDB SEGGER Jlink connected through USB.

Labels (1)
0 Kudos
Reply
1 Reply

1,190 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

I suggest you try if latest P&E or Segger FRDM-K82F board firmware can work for you:

Latest firmware application

FRDM-K82F use OpenSDA v2.1 interface, so you can refer this document to check connection configuration.

to separate the issue with specific project, I suggest you create a new project with wizard, check if the download working normally with this new created project?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply