Download problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Download problem

1,283 Views
mark_bresler
Contributor I

Hi,

Now that I have gotten my Bootloader problem solved ( Thank you Ping ), I have made a little progress, but am having a download problem.

I developed a program on my Macintosh computer ( a variant of the Red-Blue blink Carlos detailed in video 3195, to flash Red Green).

 

I get the following error message:

An error has occurred. See error log for more details.

ilg/gnuarmeclipse/debug/gdbjtag/data/CProjectAttributes

 

The Macintosh computer System Information program shows this information about the USB Bus and J-Link:

USB Bus:

 

  Host Controller Location: Built-in USB

  Host Controller Driver: AppleUSBOHCI

  PCI Device ID: 0x0aa5

  PCI Revision ID: 0x00b1

  PCI Vendor ID: 0x10de

  Bus Number: 0x04

 

J-Link:

 

  Product ID: 0x0105

  Vendor ID: 0x1366

  Version: 1.00

  Serial Number: 000621000000

  Speed: Up to 12 Mb/sec

  Manufacturer: SEGGER

  Location ID: 0x04100000 / 3

  Current Available (mA): 500

  Current Required (mA): 100

 

If someone can direct me on what to correct, it would be most appreciated,

Thanks,

Mark

Labels (1)
0 Kudos
Reply
1 Reply

1,132 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Mark,

do you use KDS3.0 or Codewarrior10.6?

if use KDS3.0, it can support  Mac OS 10.10 ("Yosemite").

Kinetis Design Studio Integrated Development |Freescale

if use CW10.6 it doesn't support Mac OS.

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply