Compatibility between KDS 3.0 and KDS3.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Compatibility between KDS 3.0 and KDS3.2

521 次查看
arvind_kumar08
Contributor I

hello 

what is the major difference between KDS3.0 and KDS 3.2?

i assume both these IDE'S are backward compatible (i.e 3.2 is compatible with 3.0).

please highlight the basic difference between the two versions.

arvind

0 项奖励
回复
1 回复

443 次查看
BlackNight
NXP Employee
NXP Employee

KDS 3.2 is basically a KDS 3.0 with all the updates/addons, see NXP Kinetis Design Studio v3.2.0 | MCU on Eclipse 

Other than that, have a look at the release notes in <install>\doc\KDS_Release_notes.pdf.

In a nutshell, they are compatible, but I recommend to use 3.2.0.

I hope this helps,

Erich

0 项奖励
回复