Compatibility between KDS 3.0 and KDS3.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compatibility between KDS 3.0 and KDS3.2

502 Views
arvind_kumar08
Contributor I

hello 

what is the major difference between KDS3.0 and KDS 3.2?

i assume both these IDE'S are backward compatible (i.e 3.2 is compatible with 3.0).

please highlight the basic difference between the two versions.

arvind

0 Kudos
Reply
1 Reply

424 Views
BlackNight
NXP Employee
NXP Employee

KDS 3.2 is basically a KDS 3.0 with all the updates/addons, see NXP Kinetis Design Studio v3.2.0 | MCU on Eclipse 

Other than that, have a look at the release notes in <install>\doc\KDS_Release_notes.pdf.

In a nutshell, they are compatible, but I recommend to use 3.2.0.

I hope this helps,

Erich

0 Kudos
Reply