Can't start debugger using J-LINK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't start debugger using J-LINK

3,157件の閲覧回数
predragvidic
Contributor I

When try to debug my project, which bilds without any problem, (Segger J-LINK) the KDS 3.2.0 replies: 'Launching my_project_name debug' has encountered a problem. Program file does not exist.

Also debugger continues to try to start and is continuously on 62%

I have followed the steps from the KDS user manual

3 返答(返信)

2,949件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Does that file you want to debug exist in the debug folder? The message indicates that it does not exist. Can you check if it exists on disk *and* in the project 'debug' folder? If it exists on disk, you might need to do a Refresh/F5 on the debug folder inside the Project view.

I hope this helps,

Erich

2,949件の閲覧回数
predragvidic
Contributor I

Thanks a lot. Helped.

0 件の賞賛
返信

2,949件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Predrag

I suggest you move this question to KDS space

https://community.nxp.com/community/mcuxpresso/kinetis-design-studio 

There are NXP KDS expert monitoring KDS space.

Jennie Zhang

0 件の賞賛
返信