Breakpoints not working after KDS/PEMicro update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Breakpoints not working after KDS/PEMicro update

2,510 Views
asfarley
Contributor IV

Hi,

I've seen a couple similar error reports but none with exactly these symptoms. 

1) Updated KDS to 3.2.0

2) Updated PEMicro KDS plugin to 3.2.4.201710241511

3) Other packages were automatically updated (GNU ARM compiler etc) although I suspect they're not the root cause

I'm using an MK22FX512VLQ12, Win10 under Mac OSX Parallels 13.

Now, my code will not stop on breakpoints while debugging. This was definitely working before. 

I have confirmed:

  • "Skip all breakpoints" is disabled
  • I've only added one breakpoint (removed all, then added 1 new breakpoint)
  • The initial startup breakpoint is working
  • Single-stepping seems to work until I hit a Wait function
  • The code with the breakpoint is definitely being executed, confirmed via UART

Anybody else encountering this? Is there a workaround or fix available? (or even a hint about what is causing this?)

I've contacted PEMicro with the same error report, will post back here if I get new information.

0 Kudos
Reply
4 Replies

2,204 Views
jairocaballero
Contributor II

asfarley‌  Have you found a solution? I have the same problem with a LPCXpresso54114 in MCU Xpresso IDE

0 Kudos
Reply

2,204 Views
asfarley
Contributor IV

Haven't looked into this again. Can you confirm: are you using a PEMicro Multilink Universal programmer?

0 Kudos
Reply

2,204 Views
jairocaballero
Contributor II

I'm using an example of SDK with a typical debugging configuration to see

the correct operation of my MCU. This under the MCUXpresso IDE. But, I

think that my problem is about incorrect debugging process, because the

example is based on FreeRTOS or similar and we have to make a debug over

the OS. See this documentation.

https://freescaleesd.flexnetoperations.com/337170/577/11781577/MCUXpresso_IDE_FreeRTOS_Debug_Guide.p...

​Thank you.​

*Jairo Andrés Caballero Peña *

E&E Eng. MsC Student

Junior Researcher & Teaching assistant

Electrical Machines and Drives - EM&D Research Group

Department of electrical and electronic engineering

Faculty of engineering

Bogotá Campus

Tel.: (57) 312 4378221 (directo)

Universidad Nacional de Colombia

http://www.ing.unal.edu.co/grupos/emd/

Volunteer - Industry Applications Society - IEEE

https://www.facebook.com/isaiasun

This message and its attachments are addressed to be used exclusive by

the recipients and it can include confidential information or legally

protected information. If you aren't the recipient, it's notified that any

distribution or reproduction of this material is prohibited. If you have

this message in error, please immediately notify us and delete the original

text including the attachments, or delete any reproduction of this. The

opinions expressed in this e-mail are exclusive responsibility of sender

and it not necessarily represents a institutional position of the

Universidad Nacional de Colombia, the use of this informaion made by the

recipient doesn't compromise the institutional responsibility. This message

have been checked with antivirus software; accordingly, the Universidad

Nacional de Colombia doesn't be responsible by the virus presence or

malicious software here, or in the attachments that could make damages.

Please, before printing this e-mail think if is truly necessary make it. Caring

for the environment and making a better world are our responsibility.

2017-11-21 12:37 GMT-05:00 asfarley <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Breakpoints not working after KDS/PEMicro update

reply from Alexander Farley

<https://community.nxp.com/people/asfarley?et=watches.email.thread> in *Kinetis

Design Studio* - View the full discussion

<https://community.nxp.com/message/963252?commentID=963252&et=watches.email.thread#comment-963252>

0 Kudos
Reply

2,204 Views
asfarley
Contributor IV

Well, I'm not sure what I was experiencing but my PEMicro Multilink/KDS combination seems to be working again. I'm able to place and hit breakpoints as expected. 

I haven't been using FreeRTOS or thread-aware debugging, so I think we're probably seeing different issues. 

0 Kudos
Reply