After we released the "Kinetis Bootloader to Update Multiple Devices in a Network for Cortex-M4" (Kinetis Bootloader to Update Multiple Devices in a Network for Cortex-M4 ), many customers want to port it to FRDM-K64 board, so here I share it.
- This bootloader is based on KDSv3.2.
-About the detail introduce and user guide, please refer to:
https://community.nxp.com/docs/DOC-328365
- There also some points when porting, please check the attachment.
- I attached the project source code. And also two user application projects.
Customers can refer to the application and user guide to configure your application project.
- The GUI is the same with bootloader for k22, we do not change anything.
BR
Alice