Hi,
I am working on OTA firmware to update K32L2A41VLL1A microcontroller. I am using FRDM-K32L2A4S devkit to test OTA.
I am using LPUART to transfer the firmware. My master microcontroller is nRF52840 which is running my OTA module to transfer firmware to NXP chip.
Since I am using devkit as of now, I manually put it in bootloader by pressing RESET and NMI switches present on board.
As per the Kinetis documentation, I have to send PING command first in order to initiate communication with the bootloader to send any commands. But when I send PING command, I am not receiving PING_RESPONSE back. I verified transmitted data over UART using logic analyzer. I tested the code with 9600 and 115200 baudrates.
I have attached screenshot from the reference manual of all the supported pins and peripherals by bootloader. I am using PTD2 and PTD3 pins (i.e. LPUART2 instance) as other UART pins are not exposed on devkit. I was planning to use PTA1 and PTA2 pins (LPUART0 instance).
Thanks and Regards,
Sahil