LPSPI module- keeping chip select active

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPSPI module- keeping chip select active

2,364件の閲覧回数
SK_98
Contributor I

Hi all,

I'm using LPSPI module of K32L2A41VLL1A to send/receive data to/from External flash. My requirement is to first send command data with Rx buffer null and then receive the buffer with tx null. i.e., after sending command there's a second send/receive function to retrieve the received buffer. But I'm not able to get that data. Can you help me with the configurations I have to do so that the Rx buffer data is not lost during my second transaction?

Thanks in advance!

Shri

 

0 件の賞賛
返信
1 返信

2,360件の閲覧回数
hefan
Contributor I

After send command data with Rx buffer null, lpspi pull cs high.You can Transfer with rx no null and tx no null.

RT1170,for reference:

hefan_2-1654064485616.png

hefan_1-1654064347837.png