K32 L2B vs MKL27z programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32 L2B vs MKL27z programming

2,166 Views
RicardoRuiz18a
Contributor II

I was using for very long time the mkl27z64 programming it with "Kinetis Flash TOOL" with usb connection. Is any tool similar flash tool to program the K32? Or im going to need a swd programmer.

Thank you

0 Kudos
Reply
1 Reply

2,153 Views
jh0
Contributor IV

I upgraded my project from KL27Z64 to K32L2A, and flashing from PC (over USB) with CLI blhost is the same. I also have new MCU-LINK, but for me (instead of breakpoint debugging I am using fast 4Mbps UART logging) CLI blhost is simple better.

If I remember right, K32L2B is with the same ROM USB loader as K32L2A, but you can check this in device datasheet.

0 Kudos
Reply